2008-04-08 9:12 PM
ReFlash STR9 part with a SD/MMC card
2011-05-17 12:33 AM
Can you reflash a STR9 part in circuit via a SD/MMC card ?
We would like to do this so we can program our device in the field with a PC.2011-05-17 12:33 AM
It is possible, an example would be to use bank1 as a bootloader.
This would then read the sdcard when inserted, and write contents of a file into bank0 flash. efs is a good place to start for an embedded file system: we have just used this in a mp3 project, the str9 sdcard port will be sent to efsl very soon. Regards sjo2011-05-17 12:33 AM
I have made a test build of EFSL for BANK1 and I have space problems. My ARM Flash release is about 30,5kB and i must write the bootloader application.
Should i write my own functions rather than STstdlib or should I try to minimize EFSL?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.