2024-02-28 9:10 AM
The USB PD status register is a combination of 4 registers.
The question is when read, are they interpreted as big endian or little endian?
so 0x91 0x92 0x93 0x94
0x91 = bit 0-7, or 28 - 31?
0x92 bit 8-11
0x93 ...
0x94 ...
The manual and programming guide are not clear .
2024-04-08 1:50 AM
Hello
Little endian is used:
@x91: bit [7:0]
@x94: bit [31:24]
Best regards
Nathalie
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.