2021-11-18 2:23 AM
Sir,
I am working on STM8S003F3P Controller which is interacting with LoRa SX1276 HPD Module. I have the experience of working on SPI and have enough knowledge to configure it.
I am able to write the data to SX1276 (I will tell you how).
But, while Reading the data from SX1276, SPI_DR register is always acting as follows.
If configured as input (Pulled up or High Impedance state), it is read as 0xFF
If configured as Output, it is read as 0x00 or 0xFF
Procedure to read the data is as follows
I have checked the waveforms for 3 to 5 registers using CRO and data is read accurately. but while keeping the controller in debug mode, unable to read the data in SPI_DR Register.
Tests Performed:
First two tests are showing the same results but CRO waves are accurate.
Here are the configurations performed and data handled
Configurations:
while((!((SPI->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE)) && (!((SPI->SR & SPI_FLAG_RXNE) == SPI_FLAG_RXNE))); //checking the transmission or reception
while((SPI->SR & SPI_FLAG_BSY) == SPI_FLAG_BSY);
SPI_DISABLE; //disable spi
SPI->CR1 = 0x3C; //clock divided by 256 (also tried the default divided by 2)
SPI->CR2 = 0x01; //2 line uni directional, no crc, full duplex hardware management ssi master mode
SPI->ICR = 0x00; //no interrupts used (tried with rx interrupt but still the value is 00 or ff)
Data handling:
uint8_t SPI_REG_ACCESS(REG_READ_WRITE_Typedef READ_WRITE, LORA_REG_ADDRESS_Typedef REG_ADDRESS, uint8_t REG_DATA)
{
SPI_CS_LOW; //cs low
while(!((SPI->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE)); //wait till transmit buffer empty
SPI->DR = (READ_WRITE | REG_ADDRESS); //Read or write is 0 or 1 respectively, reg_address is address of the register of sx1276
while((!((SPI->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE))); //wait till buffer empty
SPI->DR = REG_DATA; //dummy value
while((!((SPI->SR & SPI_FLAG_RXNE) == SPI_FLAG_RXNE))); //wait till transmit complete
dummynew = SPI->DR; //read received data
while((SPI->SR & SPI_FLAG_BSY) == SPI_FLAG_BSY); //wait till busy
SPI_CS_HIGH; //cs high
return dummynew;
}
2021-11-24 10:00 PM
Issue solved.
Perhaps I have trusted the hardware too much. After booting the same firmware in other module. It found to be working fine.
Thanks for the views.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.