2008-08-05 12:00 AM
2011-05-17 12:54 AM
Hello All,
I am trying to get the IAP (over ethernet) code to compile, but I am getting errors, which I would not expect. Seeing that their is project workspace created for IAR (all be it for version 4.XX). I am using an evaluation version of IAR v5.20 for ARM. One of the errors is regarding the inclusion of sys/time.h. If anyone can help, will appreciate it. Thanks in advance, FD.2011-05-17 12:54 AM
I have the exact same problem. After having EWARM convert the projectfiles, the project won't compile.
Any help to resolve this issue is gladly appreciated. Best regards Henrik2011-05-17 12:54 AM
You need to port this AN to EWARM5.20:
1.Replace the startup files(*.s) with the startup files available under: \IAR Systems\Embedded Workbench 5.0\ARM\examples\ST\STR91x\STR91xlibrary\startup 2.Use the STR91x_FLASH.icf as linker file: \IAR Systems\Embedded Workbench 5.0\ARM\examples\ST\STR91x\STR91xlibrary\linker2011-05-17 12:54 AM
Hello,
Many thanks for your reply. Appreciate it. Unfortunately this is not the problem, the problem is the libraries that cannot be found, as mentioned. I have searched through the IAR folders for any similar ones that could be used, but could not see any. Hope this makes sense. I think some of these libraries that are being complained about by the compiler, are from GNU ARM C/C, and maybe it is a case of just including them (hopefully with not much modifications). I will have to try. Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.