2005-04-07 12:18 AM
RCCR lost while clear read out protection, can we trim the value it back?
2005-04-04 6:42 AM
RCCR lost while clear read out protection, can we trim the value it back? Any program can help in this case?
2005-04-04 7:01 PM
ST EPB provide the facility to restore the RCCR value when read-out protection is disabled.
however if for a micro, its already lost, you need to do the clock calibration again manually to decide the value.2005-04-05 3:11 PM
Thanks for your help.
I understood the method to keep the RCCR, by tick the box ''ICP OPT disable'' while disable the read out protection, it is no problem. But because we missed the procedure, and about several hundred flash micro was done ....~__* May be program can trim the value by testing... I hope to have faster method. because hard to trim everyone manually...*_* Any good idea...? Thanks for your help.^2005-04-06 5:36 PM
'' several hundred flash micro was done ....~__* ''...
difficult situation !! if you have implemeted IAP then upgrade the flah, else i am not sure if there are bank-programmers available to program several micro together. if u have soldered these micros on app board...i dont know any solution..2005-04-07 12:18 AM
Sorry I am confused, if the RCCR cal values have been lost due to an erase restoring the default values is possible. Why would a calibration be required.
The factory programmed RCCR values are stored in a reserved area of the flash - only visible via ICC programming mode. This is done by disabling then reenabling the readout protection, obviously the flash will also need writing again. Do you not have a programming header on your target board? Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.