2003-11-24 8:50 PM
Programming Main flash while running from sec.
2011-05-17 2:56 AM
Hi all,
I'm trying to program the main flash (FS0 on 0x0000 to 0x7FFF), as a part of IAP Proccess. My CSIOP resids on 0x0200 and the RAM on 0x2000 to 0x3FFF. As I understand I have to map the Main Flash to data space for programming (while running from sec. flash) but overlap of main flash on RAM or I/O will give the priority to the RAM/IO so that , I succeed to program all addresses but not at the range 0x0200 to 0x02FF & the range 0x2000 to 0x3FFF. 1. Can I program the Main Flash when I map it to code space? 2. Can I disable the access of SRAM / IO from data space for the time of programming the main flash? Thank's for any answer Pini2011-05-17 2:56 AM
1 - Mapping the main flash to code space will make no difference
2 - You can disable the SRAM by paging it (PSDSOFT), and controlling the page register in your IAP. You may even move the SRAM from one location to another one. 3 - There is no way to disable or move the CSIOP. Can't you just locate it above the main flash?2011-05-17 2:56 AM
Thank you very much for your reply!
1. Your idea to use the paging to map out the RAM was successful. 2. I did it also to map out the CSIOP but it requiers a reset to chip after programming the flash. Using this way I can program all of the flash space but I expect it to be easier. [ This message was edited by: pini on 25-11-2003 17:21 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.