2009-10-14 10:17 PM
Problems with my AN2475 IAP boot loader application
2011-05-17 12:58 AM
Hi,
Does ANYONE here have a succesfully boot loader IAP running with an UART interface ( AN2475 ). If anyone have a sucessfully IAP example ( AN2475 ) running then I'm very interested to get/see this code, because I have serios big problems to remap and restart the downloaded application. I can see that many other people in this forum had the same problems like me, but I can't see any solve the problem. I'm using the IAR IDE, and the STR912 SK starterkit. I'm searching for an example of the AN2475 that works correct. Very frustrating, that such a thing like a boot loader application can cost so many problems. Can anybody at ST support wake up now, and help US here with a application example that really works, and explain exactly what's wrong with the existing AN2475. I guess many developers really need a boot loader, and it's a commen problem. Looking forward to hear from someone who can help me. Thanks Hans2011-05-17 12:58 AM
Hi,
I geuss your hardware remapping is Ok: I mean: Bank1 @ 0x0000.0000 address. Now the only problem we have notified in the AN2475 is : If you are reffering to the EWARMv4 example available throught this path: \AN2475\IAP_AN\Example1\project\EWARM Be aware of this mistake : (if you are using 256K/512KB STR9 device) + the 91x_init.s is configured for the 1_2MB products --> you have to change it to be for 256K/512KB products + the flash loader is the one for 1_2MB products -->you have to change it to be for 256K/512KB products (the default one) Otherwise there is no known problem on this Application note. Kind regrads, arm. [ This message was edited by: armmcu.engineer on 15-05-2009 15:35 ]2011-05-17 12:58 AM
Hi,
Well, I have modifyed the 91x_init.s to : #define Flash_512KB_Bank1_Boot + the flash loader is the one for 1_2MB products -->you have to change it to be for 256K/512KB products (the default one) Can you please specify the action for the flash loader in more details. Where or how can I change the flash loader??? I have these lines in 91x_conf.h #define Boot_Bank_1 #define Flash_512KB_256KB My application is running fine, until these lines : void Execute_STR9Application(void) { pFunction Jump_To_Application; FMI->BBSR = 0x0; FMI->NBBSR = 0x6; FMI->BBADR = 0x80000 >> 2; FMI->NBBADR = 0x0; /* Jump to the user application and execute it */ Jump_To_Application = (pFunction) 0x0; Jump_To_Application(); } Hope you can help me. Thanks Hans2011-05-17 12:58 AM
I have the same problem, if st workers can reply that we would be thankful.
With Regards...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.