2003-07-09 10:20 PM
2011-05-17 2:34 AM
I have e problem with ST9 emulator .I allwase get ''Connection error
(LPT1) st9+cannot enter monitor mode'' when I enter debug mode.I had this problem befor but than when I reset the software and the emulator it start workingcorrectly .Now It alwase stays with the same error after reseting software and emulator. Information about leds in the emulator: After power is on all first three leds are on (Power,Emulator reset,ST9 reset). After start debug mode , Emulator reset led turn off and after few seconds 'St9 reset' led turn off and Run led turn on and then I got the error. why run led turn on ?? Please answare urgently Regards2011-05-17 2:34 AM
This error occurs when:
- the emulator probe is connected to an application board not power on, or - the ST9 of the emulator probe, the ''emuchip'', is out of order. This can be caused by an emulator power off while the application board is power on.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.