2006-07-10 8:23 PM
2006-07-06 12:43 AM
Hi,
I have a problem with writing someting into the XPERCON register of the ST10F276. I use Tasking V8.0. I can write into it whatever I want, when I read it out I always get the value 0005hex (reset value). With other registers (SYSCON, ...) it works well. Has someone an idea what I do wrong? Regards, Juergen2006-07-06 2:10 AM
Hello Neila,
I wrote a small program for internal RAM where I set the SYSCON and the XPERCON register and with which I can have a look at these registers. For this program I modified the start.asm file and now I set the XPERCON first with 0x002C and then the SYSCON register with 0x0414. After this I read the registers and in XPERCON is the value 0x0005 (which is wrong) and in SYSCON is the value 0x00414 (which is ok). Regards, Juergen2006-07-07 1:25 AM
Hello,
You said that you are modifying XPERCON register in the start up file. So, to take into account this value, under ''Project Options---> startup'', the ''Generate System startup code and add it to project'' option must be disabled, otherwise the XPERCON register value, already defined in the start up file, will be changed and replaced by the value defined in Project Options---> startup ---> Xpercon'' during application build. Regards, Najoua.2006-07-09 8:20 PM
Hello Najoua,
I have already disabled this option. I took the generated start.asm file, modified it that the XPERCON register is set before the SYSCON register, disabled the ''Generate System startup code and add it to project'' option and added the modified file to my project. Regards, Juergen2006-07-09 8:29 PM
I forgot someting. :)
This is how I modified the file: MOV SYSCON, #0x0000 EXTR #1 MOV XPERCON, #0x002C BFLDL SYSCON, #0xFF, #0x0414&0xFF BFLDH SYSCON, #0xFF, #(0x0414>>8)&0xFF2006-07-09 10:24 PM
Hello juergen1769,
This is a normal behavior: In fact, EDE generates a *.cfg file for the debugger. This *.cfg file also defines some register initializations with the values AS defined in the register settings. The debugger uses these values to get the debug monitor up and running. So to get the debugger going with a custom startup code, you will indeed need to set some register values under the startup code SETTINGS. If you are not using the debugger (if you are executing your application from the internal flash), the XPERCON register value modified in the start up file will be taken into account. You can check this by executing your example from the internal Flash and displaying the XPERCON register content in the hyperterminal. Please let me know if this was not clear. Best regards, Najoua.2006-07-10 12:37 AM
Hi Najoua,
I don't use the debugger, I execute my program in RAM. That you can maybe better see what I am doing, I have attached my project. Regards, Juergen ________________ Attachments : Projekte.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Nb&d=%2Fa%2F0X0000000bYG%2FjGh73CwI4DHu_HIV7Mn0_fjZIskCAWWyH.3EOZeWyPk&asPdf=false2006-07-10 8:23 PM
Shame on me!
In the meantime I found out what I did wrong: I have located my program in XRAM and with setting XPEN to 0 you disable the XRAM ... :-[ Now I have located __CSTART_PR in IRAM (the rest is still in XRAM) and now it works. :-] Neila and Najoua, thank you very much for your help!!! Regards, JuergenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.