2003-10-24 1:42 AM
2003-10-18 2:39 AM
I have a problem with watchdog in Lite29:
1. When it is configured as software in option byte, and when I turn it on (bit WDGA = 1 in WDGCR register) and do not refresh the counter, it doesn't reset the mcu. 2. When it is configured as hardware in option byte it resets the mcu every time (every 2ms) and refresh the counter register WDGCR doesn't have an effect. It looks like the write to the WDGCR register doesn't work. (Address is correct and is 002Eh).2003-10-24 1:42 AM
Problem solved
if we work with crystal rezonator, and we set in option byte RC oscillator = disabled PLL32OFF = disabled PLLOFF = disabled then we must set PLLx4x8 = x8 then Watchdog work correct when this option is set x4 then Watchdog is not workingWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.