2006-12-27 8:31 PM
Problem with UART in MCBSTR9 Board
2011-05-17 12:34 AM
hai,
i am writing some data in the UART->DR register, but it is not same what i wrote. data what i send is 0-0F, but i am getting..... FF,FD,FB,FB,F7,F5,F7,F7,EF,ED,EB,EB,EF,ED,EF. i don't know why it behaves like this. here i am sending my code and expect sugessions. PLEASE HELP REGARDING THIS. REGARDS RAJ.2011-05-17 12:34 AM
hi raj,
to test the end of write you are using the flag UART_FLAG_TxFIFOEmpty. you have to check the right status register, something like UART_FR & (1<or UART_FR & (1<ciao2011-05-17 12:34 AM
hai Stevejamal,
in my program i want to transmit the data to the data register and monitor it on the hyper terminal. for this i have prepared the following code. UART0->LCR = UART_WordLength_8D | UART_Parity_No | FlowControl_None & UART_StopBits_1 & UART_FIFO_Disable; UART0->CR = UART_Mode_Tx | UART_Mode_Rx | 0x0001; com_baudrate (115200); for(i=0x0000; i<=0x000f; i++) { UART0->DR = i; while(UART_FR & (1< GPIO7->DR[0x3FC]= UART0->DR; for(j=0;j<=0xfff;j++); } while(1); } in my code i just put the data on the UART0->DR. but it is not same what i wrote. data what i send is 00-0F, but i am getting..... FF,FD,FB,FB,F7,F5,F7,F7,EF,ED,EB,EB,EF,ED,EF. if i send 00(0), then the data on UART)->DR is FF(1111 1111) if i send 01(1), then the data on UART)->DR is FD(1111 1101) if i send 10(2), then the data on UART)->DR is FB(1111 1011) if i send 11(3), then the data on UART)->DR is FB(1111 1011) if i send 100(4), then the data on UART)->DR is F7(1111 0111) if i send 101(5), then the data on UART)->DR is F5(1111 0101) if i send 110(6), then the data on UART)->DR is F7(1111 0111) so like this i am getting data. in hyper termioinal i am monitoring the related ASCII values. when i Debug my code i have observed these values in data register. from these values what i observe is my data is there, but it is ORing(|) with FF and Previous value. one more point is.. in my code i have enabled both TX and Rx (UART_Mode_Tx, UART_Mode_Rx)when i debug,i can monitor the data in UART0_DR as well as Hyper Terminal(ASCII Values). but if i enable only Tx then i can monitor the data in Hyper terminal (ASCII Values) but not in UART0_DR Register. i don't know why it behaves like this. its wonder that if u will help regarding this. thanks in advance. raj. [ This message was edited by: anuradha on 22-12-2006 11:06 ]2011-05-17 12:34 AM
I see that you use
UART0->DR = i; while(UART_FR & (1<bit7 is TXFIFO empty when you send a char the fifo is not empty! Your code fill the fifo without any check on fifo full. In my opinion is better to use while(UART_FR & (1<the DR register is shared with RX and TX. if you have LOOPBACK enable you are able to see what you are sending reading the DR register.2011-05-17 12:34 AM
hai Stevejamal,
when i enabled the loop back i can able to watch the data in UART->DR.its cool. but when i have enabled only Tx and send the data to the hyperterminal, then i could not watch the data on hyperterminal and UART->DR register. can u please send me the working example of UART. here my code is: UART0->LCR = UART_WordLength_8D | UART_Parity_No | FlowControl_None & UART_StopBits_1 & UART_FIFO_Disable; UART0->CR = UART_Mode_Tx | UART_Mode_Rx | 0x0001; com_baudrate (115200); for(i=0x0000; i<=0x000f; i++) { UART0->DR = i; while(UART_FR & (1<GPIO7->DR[0x3FC]= UART0->DR; for(j=0;j<=0xfff;j++); } while(1); thanks in advance raj.2011-05-17 12:34 AM
hi raj,
I didn't find the master and peripherals clock initialization in your demo. Could you check this settings? if you have a wrong internal bus clock the baudrate you are setting is not the ones you'd like to have. Let me know.2011-05-17 12:34 AM
Hai Stevejamal,
i have configured Fpll to 48Mhz, Fmaster=Fpll,BRCLK=48Mhz, PCLK is also 48Mhz. i have configured all clock settings in Startup file. please find an attachment. thanks & regards raj. [ This message was edited by: anuradha on 27-12-2006 11:02 ]2011-05-17 12:34 AM
Hai Stevejamal,
please send me the working example Project of UART . in my program i have configured 48Mhz clock for Fmaster, Fpll, Fpclk, Fbrclk(baudrate clock). already i have send u my code. expecting updations. thanks raj.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.