2012-06-26 8:08 PM
I am using STM8S103 to measure three channels of voltage signals named vs12, vs5 and vs3 respectively. Timer 4 is enabled to generate interrupt every 10ms and three voltage signals are measured alternately. That is, in the 1st 10ms interrupt, vs12 is measured. In the 2nd 10ms interrupt, vs5 is measured. In the 3rd 10ms interrupt, vs3 is measured, and so on. During each measurement, mcu makes 16 captures for further average processing. The measurement result will be displayed in HyperTerminal via UART.
The problem is that when only 1 channel (vs12, vs5, or vs3) is enabled, the measurement is correct. But when two channels are enabled, both channels' measurements are wrong. Could anyone have a look at the following code and give me some suggestions?The C code is described as follows.main(){ ADC1->CR1 |= (ADC1_CR1_SPSEL & (0x02<<4)); //fADC = 4 MHz ADC1->CR2 |= ADC1_CR2_ALIGN; //right aligment while(1){ // select the ADC channel if (vs_sel==0){ ADC1->CSR |= (ADC1_CSR_CH & CH_VS12); } else if (vs_sel==1){ ADC1->CSR |= (ADC1_CSR_CH & CH_VS5); } }}Timer 4 Interrupt:@far @interrupt void irq_system_tim4_ovf (void){ // If MAX NO OF SAMPLES are taken then voltage // values will not be recorded in array vs12_arr no_of_sample_vals = 0; while( no_of_sample_vals < MAX_NO_SAMPLE_VAL ) { //start ADC ADC1->CR1 |= ADC1_CR1_ADON; //ADC powered up ADC1->CR1 |= ADC1_CR1_ADON; //begin conversion //check for the EOC while (!(ADC1->CSR & ADC1_CSR_EOC)){}; //must read LSBs first if (vs_sel==0){ vs12_arr[no_of_sample_vals] = ADC1->DRL; vs12_arr[no_of_sample_vals] |= ADC1->DRH << 8; } else if (vs_sel==1){ vs5_arr[no_of_sample_vals] = ADC1->DRL; vs5_arr[no_of_sample_vals] |= ADC1->DRH << 8; } //ADC powered down ADC1->CR1 |= ~ADC1_CR1_ADON; no_of_sample_vals++; } // Update the time counter flag_10ms = 1; if (t_10ms==100){ /* 1 sec is completed */ flag_1sec = 1; t_10ms = 0; } t_10ms++; vs_sel++; if (vs_sel==3) vs_sel = 0; // Clear the flag TIM4->SR1 &=~(0x01); return;}2012-06-26 9:04 PM
Solved. Can anyone find the root cause? hah
2012-06-27 12:59 PM
So what was the problem then? :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.