2005-08-29 7:54 PM
2011-05-17 2:37 AM
I have a problem with two identical circuits that use micro st92f120. The systems work with an external quartz to 4 MHz and INTCLK 20MHz. The first one works correctly. The other system goes reset every three second ones. What can be? I have changed also micro of according to system and the quartz. I do not use wachtdog hw/sw and interrupt. Help me!!!
2011-05-17 2:37 AM
you should Connect the HW0SW1 pin to Vdd through a 1K pullup
2011-05-17 2:37 AM
Thanks Sergio!!! You have reason because it is the only one pin that it had the various voltage in the two circuits. Now they work. But the pins that I do not use, as an example AD\ DS\ RW where I must connect them? I have not connected these pins. I must connect them to Vdd or not?
2011-05-17 2:37 AM
It is always a good practice not leave floating pins
It is convenient to connect, the unused pins to Vdd or Vss, This will also improve,l the total power consumption of the chip2011-05-17 2:37 AM
Thanks for your answers and the aid.
PeppeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.