2007-03-15 5:30 AM
2011-05-17 12:34 AM
2011-05-17 12:34 AM
Hi Charlu,
to disable the interrupt you have to use VIC_ITCmd(TIM1_ITLine,DISABLE). I don't see what's the problem may be if you send me your code i can chek with you. best regards mirou2011-05-17 12:34 AM
Hi Mirou
Precisely, it is that which does not work, and which produces inopportune “reset�!. I tried in many mode, with several peripherals... I use (for the moment) the “Raisonance� tools chain with their startup file (and IRQ handler inside). Perhaps, the problem is in the “handler�. But ''raisonance'' says : ''it's from ST''....??? I have for the moment resolve the problem by changing the “Startup� of “Raisonance� and by putting correctly (...) the processor in mode “sys�. I then write a macro in� __asm… “which masks/unmask the bit “IRQ� of “CPSR�… But, I would prefer to mask only the accused IT, and not all ITs…2011-05-17 12:34 AM
Here an very simple example (among others). The software sending “key?� on “uart0�, and waits the reception of a character to start. Then a loop without end returns the value of channel 0 of the ADC read by IT. If i mask the ADC interrupt by “VIC_ITCmd (ADC_ITLine, SAYABLE)� or by “ADC_ITConfig (ADC_IT_ECV, SAYABLE)�, the program “reset� quickly. If not it turns without end. In a very different context, the IT timer produced the same problem.
2011-05-17 12:34 AM
Hi Charlu,
I tested your code. You have a problem in __io_putchar (char c) function which doesn’t work. About the problem of reset, I couldn’t see this problem in your code. Can you please send me a code which uses many interrupts in the same time so I can reproduce the problem. Can you also explain to me the utility of masking some interrupts among others and then renabling them. Regards mirou2011-05-17 12:34 AM
Hi Mirou !
?? The function __io_putchar (char c) works correctly in three different programs... It's a very simple function, in pooling mode (we used P6.6/Rx and P6.7/TX). For the little project that I gave in example, the problem seems completely solved with the compilation in “ARM� mode instead “Thumb�… But in our complete program - with several ITs - the problem persists: very rarely, and always on Timer 1, the system resets following the mask/unmask of the interrupt... I have no time, now, to make a small program to clarify the problem… We work with global IRQ mask... Regards Charlu2011-05-17 12:34 AM
Hi Charlu,
I don't see in your project the start up files can you please send them to . Regards mirou2011-05-17 12:34 AM
Hi, Mirou,
Our startup file, is this from Ride-Raisonnance (last update : BN746-P1). I have only modified the normal start to put the Arm in true ''Sys-Mode'' (lines are from Iar-startup). You find it in the attached file. regards charlu2011-05-17 12:34 AM
Hi all! I have the same problem with temporary masking interrupts.
I use int from UART0 and from Timer2. When I disable the interrupt for Timer2 in a normal program loop and enable it after short period of time (2 or 3 instructions later), sometimes the processor resets itself. I'm sure the int from UART0 does not influence this behavior. I tried to use crt0_STR91x.s posted by Charlu, but there were no difference. I use RIDE with newest Patch_BN746_P1_STR75x_STR9xStartup_061109.exe installed. Thank You for Your help. MilukWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.