2006-04-19 1:47 AM
2006-04-12 6:32 AM
Hello,
this is an IAP with download via USB. It works fine, when I debug it, but when it runs normally, it seems to be disturbed by an IRQ, because the LR-Register is overwritten. The consequence is that it branches to nirvana. It seems to occure in FLASH_WordWrite(). Best regards, Moe ________________ Attachments : FW_L000100_WaMa_Download.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtNI&d=%2Fa%2F0X0000000aP8%2FB.Kier2abUDlvnsY0fWku5HjnJaJi8c8jFmxdElXbTA&asPdf=false2006-04-17 9:56 PM
Hi,
the frequency shouldn't be the problem. It's set to 8MHz. I don't read from flash, while I'm writing it. I use remapping to copy the flash program to the ram, to run the program from the ram. Thanks, Moe [ This message was edited by: Moe on 18-04-2006 11:39 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.