2009-07-14 5:09 AM
Problem with downloading code into STR912 board
2011-05-17 2:32 AM
Hi,
I am presently trying to download my program into the STR912-SK board and during this process, the following error is appearing: Tue Jul 14 17:18:16 2009: J-Link firmware: V1.20 (J-Link compiled Jul 30 2008 11:24:37 ARM Rev.5) Tue Jul 14 17:18:16 2009: JTAG speed is initially set to: 32 kHz Tue Jul 14 17:18:16 2009: Found unique position in JTAG chain of ARM chip: DRPre = 1, IRPre = 5 Tue Jul 14 17:18:16 2009: CP15.0.0: 0x41259660: ARM, Architecure 5TE Tue Jul 14 17:18:16 2009: J-Link: ARM9, 966 core Tue Jul 14 17:18:16 2009: Software reset was performed Tue Jul 14 17:18:16 2009: Initial reset was performed Tue Jul 14 17:18:16 2009: J-Link found 3 JTAG devices. ARM core Id: 25966041(ARM9), ARM core Id: 00000000(ARM9) Tue Jul 14 17:18:16 2009: Device at TAP1 selected Tue Jul 14 17:18:16 2009: Auto JTAG speed: 1333 kHz Tue Jul 14 17:18:16 2009: Found unique position in JTAG chain of ARM chip: DRPre = 1, IRPre = 5 Tue Jul 14 17:18:16 2009: CP15.0.0: 0x41259660: ARM, Architecure 5TE Tue Jul 14 17:18:16 2009: J-Link: ARM9, 966 core Tue Jul 14 17:18:16 2009: Auto JTAG speed: 1333 kHz Tue Jul 14 17:18:17 2009: 3668 bytes downloaded and verified (2.50 Kbytes/sec) Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x00000328 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x00000330 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x00000340 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x00000388 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x00000398 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x000003E0 Tue Jul 14 17:18:17 2009: Warning: Target inconsistency detected at Memory address 0x000003F0 This warning is appearing for several other memory locations as well. I am a novice in micro-ontrollers and therefore do not have any clue why this is occurring. The same code is running fine on the simulator. I am using the J-Link-ARM-KS to download the same through the IAR Embedded Workbench IDE. Any help on how to resolve this problem would be great. Have been stuck with this problem with just too long. Many thanks in advance. With best regards, Arun AshokanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.