2007-11-29 8:41 AM
Problem with definition GPIO with UART0
2011-05-17 12:48 AM
Good afternoon,
I´m newbie here and new in working with STR912FW44. I need advice. I have a problem with correct definition gpio pins to functions for UART0. Code for UART is correct, when I simulated them, it was ok, but inicialization gpio 3.3 for RTS and 5.1 for Rx and 3.4 for Tx is incorect. When I want to use function GPIO_DeInit(GPIO3) and same for GPIO5, it didnt set gpio 3.,3.3 and 5.3, when I use that pins it doesn´t work correct. How to improve the function of that pins? Thanks Oldriska2011-05-17 12:48 AM
Hi Oldriska
Here is some code which can be used to set up RX and TX lines for UART0 use. The RTS can be set up in a similar fashion, but I don't have verified code for it. // Set UART0 - TX0 is P3.4 (2nd function) / UART RX0 is P5.1 #define MASK_FUNCTION 0x03 #define PORT_OUT_FUNCTION 0x01 #define ALT_OUTPUT_2_FUNCTION 0x02 #define ALT_OUTPUT_3_FUNCTION 0x03 #define PORT5_BIT1 0x02 SCU_GPIOOUT3 &= ~(MASK_FUNCTION << (2*4)); SCU_GPIOOUT3 |= (ALT_OUTPUT_3_FUNCTION << (2*4)); SCU_GPIOOUT5 &= ~(MASK_FUNCTION << (2*1)); SCU_GPIOIN5 |= PORT5_BIT1; Don't forget to also enable the UART using something like: SCU_PCGR1 |= UART1; // enable clocks to UART1 SCU_PRR1 |= UART1; // take UART1 out of reset Regards Mark ButcherWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.