2007-12-07 1:49 AM
Problem with definition GPIO with UART0
2011-05-17 2:31 AM
Good afternoon,
I´m newbie here and new in working with STR912FW44. I need advice. I have a problem with correct definition gpio pins to functions for UART0. Code for UART is correct, when I simulated them, it was ok, but inicialization gpio 3.3 for RTS and 5.1 for Rx and 3.4 for Tx is incorect. When I want to use function GPIO_DeInit(GPIO3) and same for GPIO5, it didnt set gpio 3.,3.3 and 5.3, when I use that pins it doesn´t work correct. How to improve the function of that pins? Thanks Oldriska2011-05-17 2:31 AM
Your Code?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.