2004-12-12 10:03 PM
Problem to turn on the Block Protection on F269
2004-11-30 12:17 PM
Good Morning, Sir!
I have problem to turn on the Block protection feature on ST10F269, And I just find out that Block protection feature never turn on. According to the application note. Is there any body can provide me some examples in assmebly which is working to turn on the block protection? Thanks and Regards. Jospeh Cheng :-[2004-11-30 7:43 PM
Hello,
Find two files flash.c and flash.h in the following link:http://mcu.st.com/modules.php?mop=modload&name=Splatt_Forums&file=viewtopic&topic=788&forum=5
They contain programming/erasing routines for ST10F269. There is a routine (but in C and not in assembler) named '' FlashProtectBlock(unsigned short Block) '' enabling the protection of the block that you want. I hope this helps you.2004-12-01 7:35 PM
Good Morning, Sir!
I have try to used the link you provided and I have download it from the web, but Actually, I can not get it working. MOV R5,#FCI3 ;Command address MOV R6,#FCI4 ;Command address %WRFCI (#RPS) MOV R13,#6 ;Odd word address MOV R7,[R13] %*DEFINE (WRFCI (EPCcmd)) ( MOV R7,#CIE1 MOV [R5],R7 MOV R7,#CIE2 MOV [R6],R7 MOV R7,%EPCcmd MOV [R5],R7 ) And I just find that When I expect I can read the Protection Regsiter, It is actually the data which I store inside the Flash. And I find something in the manual that i have to reset the Protection interface after I have read protection register for one times. Please somebody have some workable assembly to turn on the flash protection. Many Thanks for all !!!! I have work on this problem for three whole day already. :-[2004-12-12 10:03 PM
Good Morning, EveryBody!
I have finally found out that the problem is casued by I have not write a Read/Reset command after I have Read protection status. Thanks for all who have help to solve the problem. Joseph ChengWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.