2008-01-27 10:39 PM
Problem to start a new program after doing a bootloader in IAP mode
2008-01-27 10:39 PM
Hi,
After doing a bootloader to load a new program, i reset my MCU and only the code in sector 0 (main()) is executed. When the program calls the fist routine loacated in the sector 2, nothing happens. Why? Otherwise, another test what i did consists to load the same software thanks to my bootloader. In this case, there is no problem! Below, what i noticed when i change my original software located in MCU before loading again: 1) Original code in sector 2: #if DEBUG_BOOT sci_Send_Byte_Boot(0xA1); #endif becomes #if DEBUG_BOOT sci_Send_Byte_Boot(0xA2); #endif In this case, after loading this new program, no problem! But now, if i add some new lines in my new software: #if DEBUG_BOOT sci_Send_Byte_Boot(0xAA); sci_Send_Byte_Boot(0xA2); sci_Send_Byte_Boot(0xBB); #endif In this case, the first routine in sector 2 is not called. Maybe it's due to the changing of memory size? Below, a comparison between the original and new map file (only the beginning of sector 2 which begins to 0x1000 adress): New: Init_sector2 1000 3 ( 1) CODE INIT_SECTOR Loop 1003 8 ( 1) CODE LOOP_SECTOR interrupt_timerA 1020 26 ( 0) CODE CALL_VECTOR10 main_run 1046 86 ( 1) CODE FUNCS main_task 10CC 3 ( 1) CODE FUNCS main_serial 10CF 114 ( 2) CODE FUNCS Original: Init_sector2 1000 3 ( 1) CODE INIT_SECTOR Loop 1003 8 ( 1) CODE LOOP_SECTOR interrupt_timerA 1020 26 ( 0) CODE CALL_VECTOR10 main_run 1046 7C ( 1) CODE FUNCS main_task 10C2 3 ( 1) CODE FUNCS main_serial 10C5 114 ( 2) CODE FUNCS Regards, Nicolas [ This message was edited by: nicolas_homeostasie on 28-01-2008 12:13 ] [ This message was edited by: nicolas_homeostasie on 28-01-2008 12:14 ] [ This message was edited by: nicolas_homeostasie on 28-01-2008 12:15 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.