2014-05-16 7:19 AM
Hi everyone
I am using STM8S003F3 in my board. for reading 5 analog inputs in regular interval I have used single conversion - scan mode - buffered ADC triggered by TIM1 by the following code//ADC1_DeInit ();
ADC1_Init ( ADC1_CONVERSIONMODE_SINGLE, ADC1_CHANNEL_6, ADC1_PRESSEL_FCPU_D18, ADC1_EXTTRIG_TIM , ENABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_ALL, DISABLE ); ADC1->CR2 |= ADC1_CR2_SCAN;//ADC1_ScanModeCmd ( ENABLE ); ADC1->CSR |= (uint8_t)ADC1_IT_EOCIE;//ADC1_ITConfig ( ADC1_IT_EOCIE, ENABLE ); ADC1->CR3 |= ADC1_CR3_DBUF;//ADC1_DataBufferCmd ( ENABLE ); ADC1->CR1 |= ADC1_CR1_ADON;//ADC1_Cmd ( ENABLE ); and I configured TIM1 to trigger ADC1 in regular times with the following code//TIM1_DeInit ();
TIM1_TimeBaseInit (TIM1_PRESCALER, TIM1_COUNTERMODE_UP, TIM1_PERIOD, 0); // TIM1_ITConfig (TIM1_IT_UPDATE, ENABLE); TIM1->CR1 |= TIM1_CR1_ARPE;//TIM1_ARRPreloadConfig (ENABLE); TIM1_SelectOutputTrigger (TIM1_TRGOSOURCE_UPDATE); TIM1->CR1 |= TIM1_CR1_CEN;//TIM1_Cmd (ENABLE); when I run my program, it works normal for at least 30 seconds, after that the ADC buffer values get zero!!! it seems that all interrupts are working correct. A new clue that I found is that, ADC overrun flag is always SET from the start and as I checked, ADC triggering by TIM1 is slow enough to avoid over running! ( I even make triggering 10 times slower ) Even if I clear the over run flag, it gets SET again. I think buffer over running stops ADC from conversion input channels but I don't know how I can deal with this I appreciate if you give me your comments #stm8s-adc1-scan-mode #adc-stm8 #stm8-adc-problem2014-05-23 4:22 AM
I caught the problem!!!
It seems to be a hardware exception, because ADC EOC ( end of conversion ) interrupt works but ADC content is zero. I replace TIM1 external trigger ( which was hardware act ) with TIM1 interrupt, in which I do ADC1 start conversion ( a software act ), and the problem disappeared! I think the following failure had been taking place: in my code, the whole operations are performed in interrupt routines, but the TIM1 external trigger was triggering ADC1 by hardware without seeing if the other interrupt routines had been done and released CPU resource before ADC1 EOC ( end of conversion ) handler can read the results. so in particular intervals ADC1 was being triggered by TIM1 before ADC data buffers had been read. I thought this would just raise an overrun flag but in practice, the repetition of this phenomena took ADC1 hardware to a permanent state in which it was returning zero for nonzero analog inputs. I would be thankful if anyone, specifically a ST company expert, say his/her opinion about this2015-12-19 3:24 AM
Hi abbas,
I am working on sensing of my AC waveform (of 50 Hz) with ADC1 of STM8S003k3 MCU.I want to trigger my ADC with TRGO event from TIM1.
The TRGO signal is my OC1REF signal.When i observed my Timer Ouput(TRGO) on PC.1 pin,i am getting correct sampling freq set by me(10 Khz).But i am not able to get correct sampled waveform.So i am in doubt that my TRGO event is triggering my ADC correctly or not.
Following is my TIM1 setup: TIM1->CR1 &= ~0x10; // upcount counter TIM1->ARRH= (u8)(AUTORELOAD >> 8); // init sampling period and pulse wide TIM1->ARRL= (u8)(AL); // auto reload register TIM1->CCR1H= (u8)((AUTORELOAD) >> 8);// compare register TIM1->CCR1L= (u8)(AL-AD_STAB); TIM1->CR1|= TIM1_CR1_ARPE; // auto reload register is buferred TIM1->CR2 |= 0x40; // CC1REF is used as TRGO TIM1->CCMR1= (6<<4) & TIM1_CCMR_OCM; // CC1REF in PWM 1 mode TIM1->IER |= TIM1_IER_CC1IE; // CC1 interrupt enable TIM1->CCER1|= TIM1_CCER1_CC1P; // OC1 negative polarity TIM1->CCER1|= TIM1_CCER1_CC1E; // OC1 output enable TIM1->BKR|= TIM1_BKR_MOE; TIM1->SMCR|= TIM1_SMCR_MSM; // synchronization of TRGO with ADC TIM1->CR1|= TIM1_CR1_CEN; // timer 1 enableTIM1 Interrupt:-INTERRUPT_HANDLER(TIM1_CAP_COM_IRQHandler, 12){ GPIOD->ODR &= ~PIN_0; TIM1->SR1&=~TIM1_SR1_CC1IF; ADC1->CR1 |= ADC1_CR1_ADON; }I am reading my ADC conversion on EOC IE interrupt.
Please help me regarding this.It is very important for me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.