2005-06-01 3:59 AM
2011-05-17 3:07 AM
Hello!
what is the difference whit the I/O port of MCU P1,P3,P4 and the I/O port OF PSD PortA, PortB,PortC, PortD2011-05-17 3:07 AM
There are pretty significant differences. The MCU ports (P1, P3, and P4) basically have the same electrical characteristics as the Intel 8032AH MCU. This means that they're TTL-compatible and not CMOS technology. The PSD ports ARE CMOS ports which means that have much higher Voh and lower Vol. Additionally, they're capable of sinking / sourcing far more current than the MCU ports. Finally, the PSD ports can interact with the programmable logic to automatically serve different functions (chip selects, etc.).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.