2017-10-01 3:08 PM
I have a mother board of audio, video and gps with STM8S207K6 MCU that is working condition. When I try to read eeprom from the device, the message will appear 'Can not communicate with the device.
Check the swim cable connection and check all the needed pin connection or the swim connecter
If the application code uses swim desable and reset pin as out put or has desabled swim clock driver Try now to switch off and on the application power while nrst pin forced low'All pins are connected with same as mentioned .
Pins of Swim, Nrst, VDD and GND.
2017-10-02 7:06 AM
Sorry what's the question here?
Is this a device, board or software you designed, or worked on, or someone elses?
2017-10-02 2:18 PM
A device with read-out protection would preclude you from accessing or debugging.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.