Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L050J3 Bug?

Hi,I am experiencing a serious problem with STM8L050J3.Due to an unused pin configuration of port A (PA1..PA7) then excluding PA0 used as SWIM, in order to check for any difference in current consumption, I have configured Port A with the following c...

With STM8S005C6 How to program ADC Interrupt with a range of ADC_WG with continuos mode, with the scanning?

Hello, I would like help to have configurating the ADC peripheric to use it in continuos mode with three channels of the micro stm8s005c6, could you hand me an example made with the FWL from ST? Im using it right now with no success.I have being read...

SBosc by Associate II
  • 1030 Views
  • 0 replies
  • 0 kudos

Why getting such error though code looks error free ? #error cpstm8 ..\..\src\main.c:350(0+6) misplaced local declaration #error cpstm8 ..\..\src\main.c:411 static function monitor_express_open_input_button undefined

static bool isEOBtnPressed = FALSE;static bool isECBtnPressed = FALSE;static void monitor_d_input_button(void); /*PB1 pin as input pin pull-up mode*/static void monitor_o_input_button(void);/*PB2 pin as inputpin pu;;-up mode*/static void monitor_c_in...

AAnsa.2 by Associate
  • 2455 Views
  • 2 replies
  • 0 kudos

Can JTAG pin 19 VDD (out) be connected directly to SWIM VDD (sense) to power STM8 MCU's from ST-LINK /V2 when programming?

It has been weakly suggested in other threads, but I would appreciate a firm confirmation. Does anybody have first-hand experience doing this?Is anything else required? For example connecting the grounds of the SWIM and JTAG? (Hard to guess the corre...

lyoy by Associate III
  • 1445 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.