2007-08-27 9:39 PM
2007-08-27 1:33 PM
Hi,
The Help says that when programming the CPU with the option byte disabled, the option byte in the CPU is ignored. How does the CPU know if I am using option byte disabled or enabled? Does it check the ICCCLK and ICCDATA at start? Also, if my CPU has been programmed to use ResonatorOscilator and I want to use Option byte disabled (which means the programming tool will be providing the clock), do I need to disconnect the CPU from its current clock source Thank you2007-08-27 9:39 PM
A different number of pulses is used to enter each programming mode.
No you do not need to disconnect any clock source. Regards SpenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.