2005-10-13 11:59 PM
2005-10-04 8:42 AM
Hello
if I program TIMER as OUTPUT MODE TOUT= 1 and DOUT =1 or DOUT = 0 should I program in the OPTION BYTE the TIM PULL bit as 0 (disabled)? If I program as TIMER PULL UP =1 enabled what happen? Destroy the device? Increase the power consumption? Thanks Ghip2005-10-13 11:59 PM
It will not cause any damage to the device but is not recommneded as pull up feature is for input mode(Tout = 0)
When Tout = 1 , the pull up is disabled even if the option is enabled.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.