2025-01-09 3:11 AM - last edited on 2025-01-09 5:26 AM by mƎALLEm
Hi,
2025-01-14 1:01 AM
Or overestimated the capabilities of the developers?
Surely, scaling is going to be simpler (therefore, quicker & less code) than fixed-point ... ?
2025-01-14 4:45 AM
> Or overestimated the capabilities of the developers?
That could very well be, too.
Although I most often experienced the former issue, project managers going as cheap as possible. And not only once have I seen the grudging "upgrade" to a bigger, more expensive MCU variant, more often for code space issues than performance issues.
But I think this is a critical point some developers and project managers did not understand. Cortex M is general-purpose application architecture, not optimized for high-throughput (like DSPs). High data rates and interrupt frequencies (like for cycle-by-cycle control) can quickly stuff the core, and eat up 80...100% processing time. And no matter if you throw more expensive hardware (M7, dual core) at it or more specialized / optimized hardware (DSPs), it will not come cheap.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.