2003-09-01 6:52 PM
2003-08-21 1:33 AM
Hi,
I have problem programming the NMI pull-up on ST62T32B with winee 4.0.2 When I set 'D2 NMI pin pull-up enabled' to 1 (ON) there is no pull-up present on the NMI pin. But if I set 'D2 NMI pin pull-up enabled' to 0 (OFF) and 'D3 TIMER pin pull-up enabled' to 1 (ON) there is a pull-up on the NMI pin !! It seems to me that the bits D2-D3 are mixed up. Am I right or is it my brain thats mixed up? Regards Bood2003-09-01 6:52 PM
You are right, D2 and D3 Bits are explained reversed in the datasheet. In Actual , bit D2 is used to pull up Timer pin and D3 to pull up NMI Pin.
The datasheet will soon be modified accordingly. Thanks for your help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.