2007-11-04 8:13 PM
Newbie to ARM. Please help to my first program.
2007-11-02 6:12 AM
Hello all,
I'm newbie in ARM microcontroller :) and I'll be pleased if you could help me with my first program. In order to enable UART1, the code I write is: GPIO_Config(GPIO0,0x0800,GPIO_IN_TRI_CMOS); GPIO_Config(GPIO0,0x0400,GPIO_AF_PP); UART_OnOffConfig(UART1, ENABLE); UART_FifoConfig (UART1, DISABLE); UART_FifoReset (UART1 , UART_RxFIFO); UART_FifoReset (UART1 , UART_TxFIFO); UART_LoopBackConfig(UART1 , DISABLE); UART_Config(UART1,9600,UART_NO_PARITY,UART_1_StopBits,UARTM_8D); It returns to me an error: Undefined External RCCU_FrequencyValue refered in UART... What is worng? Do I need to add something else? Please help me. Best regards. Alfa2007-11-04 8:13 PM
Missed library, solved.
forget it please. AlfaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.