2008-12-26 2:44 PM
Need some help creating an IAP app
#iap #bootloader #upsd32532011-05-17 3:04 AM
hey! i am not sure if this thread is still active. but i have read through some of the information in this thread. anyway, i would like to ask if its possible to send me some of the sample files (boot loader, etc) to my e-mail add.
mailto:zoro7117@gmail.com
thank you very much....2011-05-17 3:04 AM
Zip file on the way...
2011-05-17 3:05 AM
mulls,
thanks for the zip files. i am fairly new to this stuff and it might take a while for me to be able to understand the discussions in this thread.2011-05-17 3:05 AM
has anybody have tried doing IAP with PSD423G2 and Infineon Microcontroller C161CS? thanks.
-roger-2011-05-17 3:05 AM
hey guys i need your help....
i have read through the thread a couple of times, and read through a lot of documents in the ST website, but i still cannot get into motion. concept wise i have understood how you guys implemented your IAP, but the big difference is that i am currently using a C161CS microcontroller (which is a 'von neuman' architecture, and different instruction set from 8051 mcu - also, i am a newbie in assembly and embedded programming in general.) anyway, here is my current configuration: (hardware) 1. mcu - c161cs 2. psd - psd4235G2 in my keil project, my external memory settings are the following: # type start end 1 ROM 0x0 0xFFFF 2 ROM 0x10000 0x1FFFF 3 RAM 0x20000 0x220FF 4 RAM 0x30000 0x6FFFF in my PSD project, my current configuration is the following: fs0 = 0x0000 - 0xFFFF fs1 = 0x10000 - 0x1FFFF rs0 = 0x20000 - 0x21FFF csiop = 0x22000 - 0x220FF anyway, the above configuration is for my main application. but after this configuration, i am stuck... 1. i do not know how to configure my memory map for IAP, in keil and PSD as well... 2. i cannot duplicate/copy your startup code, to try if my switching from main apps to iap apps work, because of different instruction set. aside from the docs that mulls sent me, i have downloaded and read other documents, but still it seems i have been moving 1 step forward and 2 step backwards. anyway, hopefully you have some fresh ideas that i can start to work with... thanks.2011-05-17 3:05 AM
Hi mulls,
I'm new to micro PSD. I'm developing IAP for 3254.I read the previous messages in this thread.Could you please send the zip files to me.mail id ismailto:achaitanya@mic.co.in
. Thanks and Regards, Chaitanya2011-05-17 3:05 AM
2011-05-17 3:05 AM
Dear All,
This post was a Great Help. We were successful in implementing the same and are currently in production. Previously we were using the UPSD3354D-40U6 with battery backup of internal SRAM, but now we are using the UPSD3354D-40U6 without battery backup of internal SRAM as this feature was removed by ST. So we are using external SRAM with battery backup with appropriate changes in the Keil project.Now we are facing an issue where sometimes the Bootloader Application (IAP mode) is executed instead of the Main Application. This happens either on power on or the Watchdog reset. As the Application is programmed normally and the sttus Byte is set, and the SRAM Key location has the RUN IN MAIN string, mostly the Main Application is executed but its sometimes with unknown reasons the Bootloader Application (IAP mode) executed. We have lot many boards with same issues. We have few boards where this isn’t ever observed.
I check the code several times but could not find any thing. can it be related to turbo mode? we have not changed the default mode. Thanks2011-05-17 3:05 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.