2007-04-23 4:24 AM
Message for all curious about end of write interrupt
2007-03-29 10:42 PM
Unfortunately the end of write interrupt doesn't work you need to test the relevant bit as managed in standard library.
Nice and efficient way would be also using timer so you won't waste your time by wait loop and you would get dedicated time frame for testing bit according to the ammount of data to be written. I'm sorry about that information I beliave we'll solvve the issu in the next revision. Regards Radim2007-04-01 9:37 PM
Thank you for the information. It is good to see communication going between us, developers, and the MCU manufacturer.
Now would probably be a good time to issue an official errata document. Best regards, - mike2007-04-02 2:46 AM
Hello,
we are investigating on the issue and thanks for all your details. We reproduced the problem of end of write operation but ONLY when using running in Debug Mode: - If a Global run is applied, there is no problem: the End Of Write Interrupt is serviced normally. - If Breakpoints are inserted in the project and ‘Step Over’ or ‘Step Into’ are used, the problem could occurs. In stand-alone, there is no problem: the End Of Write Interrupt is serviced normally. We are also using the toolchain IAR 4.40 and other tests are set to find precisely the root cause. Thanks for your understanding. We will keep you informed with our last results and the root cause of this behavior.2007-04-02 3:35 AM
Hello,
I would suggest the following test: 1) Clear the flash channel interrupt enable flag: EIC_IER0.IER1 = 0 2) Perform a flash write to trigger the flash interrupt 3) Wait until the flash write operation is completed 4) Execute a delay, say 10 milliseconds to be sure 5) Set the flash channel interrupt enable flag: EIC_IER0.IER1 = 1 6) Observe Expected result: after step 5 an interrupt should trigger Actual result: no interrupt is triggered Further tests: Reduce the delay in step 4 above until the interrupt starts to trigger. Needless to say, the tests should be run uninterrupted (by the debugger or anything else). Best regards, - mike2007-04-04 2:55 AM
Hello Volius,
Could you please give me a compiled project reproducing the problem? Regards, Najoua.2007-04-04 3:16 AM
This might take me some time. I will try to put together a project reproducing the problem this week and post it to this thread.
Regards, - mike2007-04-04 3:19 AM
Ok,thank you Volius. I am waiting for your feedback.
Regards, Najoua.2007-04-05 6:10 AM
Hello Najoua,
Please find attached a compiled project demonstrating the problem. Regards, - mike ________________ Attachments : flash_test.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtHs&d=%2Fa%2F0X0000000aL6%2FbFgXhrftr26cROHQdUkPwW57lwEhiQvEXoW30A2q0B8&asPdf=false2007-04-05 8:48 PM
Hello Volius,
Could you please provide me the iostr710.h header file because it doesn't exist in the IAR version I have. Thank you in advance, Regards, Najoua.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.