2010-12-04 11:02 PM
Meaning of Cosmic's segment .bss size overflow error
2011-05-17 6:11 AM
Hi,
1744 is the size of the overflow, that is, the difference between the actual size of the segment and its maximum size (as specified by the -m parameter for that segment, in the linker file) As for your other question, I quote the user manual, page 9:The COSMIC compiler defines the __CSMC__ preprocessor symbol.... Regards, Luca PS: note that when you have a linker error the map file is NOT created.2011-05-17 6:11 AM
Thank you, and succinct.
The page 9 reference (I had read it) escaped my understanding as to its ability to discern the Cosmic compiler. Perhaps a mention could be included in the manual?
2011-05-17 6:11 AM
''The page 9 reference (I had read it) escaped my understanding as to its ability to discern the Cosmic compiler.''
It seems pretty clear to me - in what way would you have it changed?''Perhaps a mention could be included in the manual?''Which manual do you mean?
Since the Standard Peripheral Library supports both Cosmic & Raisonance compilers, its source code would seem like an obvious place to look to see how it distinguishes the two; eg, in stm8s.h:
/******************************************************************************/
/* Library configuration section */ /******************************************************************************/ /* Check the used compiler */ #if defined(__CSMC__) #undef _RAISONANCE_ #define _COSMIC_ #define TINY @tiny #define NEAR @near #elif defined(__RCST7__) #undef _COSMIC_ #define _RAISONANCE_#define TINY page0
#define NEAR data #else #error ''Unsupported Compiler!'' /* Compiler defines not found */ #endifWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.