2022-03-18 10:13 AM
I am trying to get I2C communication working between two STM8S003F3P6.
From I2c master I am trying to initiate I2C start message using CR2 registers with below code
#define I2C_CR2_START ((uint8_t)0x01) /*!< Start Generation */
.....
I2C->CR2 |= I2C_CR2_START;
But executing I2C->CR2 |= I2C_CR2_START; immediately restart and it keeps crashing at the same line.
Can someone please help what is possible cause of it, and how to get over this issue
2022-03-18 11:27 AM
STM8 support here is not so good. I have two cases and no response.
Unless I2C->CR2 address is wrong, the problem is not in that line. You should put here more details, more code, not just one line. Also it seems that you should read RM0016 with more attention.
My guess is that the problem is in an ISR that is executed after that line is executed.
2022-03-18 10:13 PM
I see correct address gets generated in asm file below
; src/main.c: 173: I2C->CR2 |= I2C_CR2_START;
ld a, 0x5211
or a, #0x01
ld 0x5211, a
Below is the interrupt handler defined , but I do not see that getting invoked as print statement does not get executed below
INTERRUPT_HANDLER(I2C_IRQHandler, 19)
{
printf("I2C_Interrupt \n");
switch (I2C_GetLastEvent())
{
/* EV5 */
case I2C_EVENT_MASTER_MODE_SELECT :
#ifdef TEN_BITS_ADDRESS
/* Send Header to Slave for write */
I2C_SendData(HEADER_ADDRESS_Write);
break;
/* EV9 */
case I2C_EVENT_MASTER_MODE_ADDRESS10:
/* Send slave Address for write */
I2C_Send7bitAddress(SLAVE_ADDRESS, I2C_DIRECTION_TX);
break;
#else
/* Send slave Address for write */
I2C_Send7bitAddress(SLAVE_ADDRESS, I2C_DIRECTION_TX);
break;
#endif
/* EV6 */
case I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED:
if (NumOfBytes != 0)
{
/* Send the first Data */
I2C_SendData(TxBuffer[Tx_Idx++]);
/* Decrement number of bytes */
NumOfBytes--;
}
if (NumOfBytes == 0)
{
I2C_ITConfig(I2C_IT_BUF, DISABLE);
}
break;
/* EV8 */
case I2C_EVENT_MASTER_BYTE_TRANSMITTING:
/* Transmit Data */
I2C_SendData(TxBuffer[Tx_Idx++]);
/* Decrement number of bytes */
NumOfBytes--;
if (NumOfBytes == 0)
{
I2C_ITConfig(I2C_IT_BUF, DISABLE);
}
break;
/* EV8_2 */
case I2C_EVENT_MASTER_BYTE_TRANSMITTED:
/* Send STOP condition */
I2C_GenerateSTOP(ENABLE);
I2C_ITConfig(I2C_IT_EVT, DISABLE);
break;
default:
break;
}
}I checked in my code at below locations, its master thats failing,
https://github.com/spsarolkar/stm8s-i2c-master
https://github.com/spsarolkar/stm8s-i2c-slave
I am using sample example code for I2c from standard peripheral library STM8S_StdPeriph_Lib/Project/STM8S_StdPeriph_Examples/I2C/I2C_TwoBoards/I2C_DataExchange
2022-03-19 3:22 AM
You should not use printf in an interrupt handler. Maybe this is the problem.
2022-03-19 7:41 AM
I removed it from interrupt routien now but still same result, below output keeps repeating indicating restarts at I2C_GenerateSTART each time
checking function state done �I2C_DeInit
I2C_ITConfig
enableInterrupts
TxBuffer
I2C_GenerateSTART
checking function state
checking function state done �I2C_DeInit
I2C_ITConfig
enableInterrupts
TxBuffer
I2C_GenerateSTART
checking function state
checking function state
2022-03-19 12:23 PM
Maybe the problem is stack.
If not put a while(1) forever loop in interrupt handler in several places to force program to stop. If it stops, means no restart, problem is in next lines.
Or use a debug build and place breakpoints. But you need to use STVD.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.