2007-06-13 5:22 AM
2007-06-13 2:50 AM
Hello, on the homepage of ARM stands that the ARM7TDMI has an interface for a COprocessor. Is it possible to attach to the STR7 mathematical CO a processor?
Are there are any restrictions, which coprocessor I can use. And wheredo i get such Co-Processors?[ This message was edited by: hugo123 on 13-06-2007 15:34 ]2007-06-13 5:22 AM
Hi hugo123,
I think that ARM7TDMI core built in STR7 is isolated from the extern environnement (the microcontroller package), so I think that there are no external interface to a specific co-processor. However, if there are any co-processor which able to communicate with EMI (External Memory Interface), I think it is possible in this case to interface it with STR710 EMI interface.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.