2025-11-20 1:24 AM
Hello,
I have an issue reading and writing to and from the M95P32. So far it has never worked. I tried using the official ST driver https://github.com/STMicroelectronics/stm32-m95p32/tree/main but nothing happened. I don't know if the write was successfull but when I tried to read back the data, I only receive 0x00.
Here is a sample of the code used
#define USE_SPI
#include "m95p32.h"
std::int32_t eeprom_init() {
return 0;
}
std::int32_t eeprom_deinit() {
return 0;
}
std::int32_t eeprom_read( uint8_t *data, uint8_t size ) {
silentlib::spi_lock cs_pin{ device::instance().eeprom_cs };
return HAL_SPI_Receive( &hspi3, data, size, 1000U ) == HAL_OK ? 0 : -1;
}
std::int32_t eeprom_write( uint8_t *data, uint32_t size ) {
silentlib::spi_lock cs_pin{ device::instance().eeprom_cs };
return HAL_SPI_Transmit( &hspi3, data, size, 1000U ) == HAL_OK ? 0 : -1;
}
std::int32_t eeprom_sendrecv( uint8_t *data_transmit, uint8_t *data_receive, uint16_t size ) {
silentlib::spi_lock cs_pin{ device::instance().eeprom_cs };
return HAL_SPI_TransmitReceive( &hspi3, data_transmit, data_receive, size, 1000U ) == HAL_OK ? 0 : -1;
}
void eeprom_delay( uint32_t amount ) {
silentlib::delay_ms( amount );
}
// snip
int main() {
MX_SPI3_Init(); // 500kHz; CPOL = 0; CPHA = 0;
// ...
M95_Object_t eeprom {
.IO = {
.Init = eeprom_init,
.DeInit = eeprom_deinit,
.Read = eeprom_read,
.Write = eeprom_write,
.SendRecv = eeprom_sendrecv,
.Delay = eeprom_delay,
.Address = 0x00,
},
};
std::uint8_t message_to_write[] {"Test M95P32"};
const std::size_t address_to_write {};
std::uint8_t message_to_read[ 128 ]{};
const std::size_t address_to_read { address_to_write };
Page_Write( &eeprom, message_to_write, address_to_write, std::size( message_to_write ) );
Single_Read( &eeprom, message_to_read, address_to_read, std::size( message_to_read ) );
// message_to_read => 0x00
}We pulled up the CS line to VDD line ( ~3.5V ) of the EEPROM with a 47kohm resistor instead of 100kohm.
HOLD and WP pins are held high.
Is there anything I forgot ?
Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.