cancel
Showing results for 
Search instead for 
Did you mean: 

M24C04-DRMF3TG/K thermal resistance data

abordonali3
Associate

I am performing a thermal analysis with component M24C04-DRMF3TG/K TSSOP8 package.  The datasheet does not contain any of the typical thermal resistance information:  thetaJA, thetaJC_bottom, thetaJC_top.  Is this information available?  

Thanks,

Andrea

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @abordonali3,

The same answer that has already been given here applies here as well. However, the memory size of your M24C04 is smaller by a factor of 512, so that the maximum power loss incurred is about 50 times smaller, even at the slowest speed of 100kHz. Since this is already negligible there, it is even more so for this small M24C04.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @abordonali3,

The same answer that has already been given here applies here as well. However, the memory size of your M24C04 is smaller by a factor of 512, so that the maximum power loss incurred is about 50 times smaller, even at the slowest speed of 100kHz. Since this is already negligible there, it is even more so for this small M24C04.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.