Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to reset Tx CRC calculator properly?

My application uses a STM8AF5288 as SPI slave with hardware Rx and Tx CRC calculator enabled.Despite the information available on the Ref Manuals, just writing '1' to CRCEN bit of SPI_CR2 seems to work only on SPI_RXCRCR.SPI_TXCRCR will not reset wit...

AFerr.1 by Associate II
  • 1137 Views
  • 0 replies
  • 0 kudos

Is the MOSFET (STP85NF55L) reliability affected if the Vgs is near to the maximum specified in the datasheet?

My customer specifies a relation of 60% of the maximum Vgs for operation. My design is using 80% of the maximum Vgs. They are asking how this increase will affect the component reliability (failure mechanism, failure rate...).My design is eqquiped wi...

IGent.1 by Associate
  • 708 Views
  • 0 replies
  • 0 kudos

ST-LINK does not see Option Bit HSITRIM (Old name 16MHZTRIM0) in uC ST8AF6246. IDE is IAR. How to set this bit?

Hello, I use ST-LINK to set Option Bytes in uC ST8AF6246. IDE is IAR.I have a trouble with Option Bit HSITRIM (Old name 16MHZTRIM0). According to uC datasheet this bit allows oscillator trimming with 3 or 4 bit resolution (One bit for sign). ST-LINK ...

nord11 by Associate
  • 683 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.