2005-01-19 8:50 PM
2005-01-19 12:19 AM
Hi all
Can any body help me out with SPI code as i am new to this . Looking forward for the code, Thanks in advance2005-01-19 11:27 AM
Are you talking about software or hardware spi ?
Have a look at the following appnotes in the download section AN 970, AN 972 and also the st7 library Regards sjo2005-01-19 7:56 PM
Hi
i am talking about the software SPI which will help in communicating MCU with the External components on the board. thanks2005-01-19 8:50 PM
AN972 gives details of a software spi master, a slave device is a lot more complicated and would be better done using the hardware spi cell. Can you not use this as it is present on all st7's
Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.