2011-02-05 1:02 AM
Can you help me - when I build example stm8l discoevry. dev - linker returns error:
Running Linker
clnk -l''C:\Program Files\COSMIC\CXSTM8_32K\Lib'' -o Debug\discover.sm8 -fakeSemiAutoGen -mDebug\discover.map Debug\discover.lkf
clnk: unknown option -fakeSemiAutoGen
The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_32K\Lib'' -o Debug\discover.sm8 -fakeSemiAutoGen -mDebug\discover.map Debug\discover.lkf '' has failed, the returned value is: 1
exit code=1.
discover.elf - 2 error(s), 0 warning(s)
Where can be my problem?
Thamks,
fj
2011-03-22 5:08 AM
Hi John,
I think this error is related to the license file from Cosmic. Do you have the license.lic file for the 32K free version? Regards, Joan2011-03-22 5:24 AM
Hi John,
In the STVD project settings, select your Cosmic license path (probably the 16K) by browsing the good root patch : C:\Program Files\COSMIC\CXSTM8_16K. The priginal project workspace has probably been saved with 32K license settingd. best regards2011-11-26 9:12 AM
Dear stefast,
first - thanks for your answer!, but mypoblem is not solved. I have licensed both 16k+32k Cosmic. (when I do change to 16k, linker send the same error.... Have you any other idea how solve my problem, please ? (I have not worked on STM8L some time, because there were many other projects... and now I can not start work again...) Best regards, johnWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.