2023-11-15 8:31 PM
we used L99DZ200 for gate driver for running 2ea DC motor at the same time.
if there is induce voltage from one motor with H-bridge(FET body diode) due to generating mode by external load(example by hand), and the other motor is connected to other side H-bridge,
could the other motor work by that induce voltage which is made by one motor in terms of gate driver?
our design circuit is like below picture.
2023-11-23 6:15 PM
could you answer to me about this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.