2016-09-30 3:05 AM
I have an issue with a STHVDAC-253M which provides 0 to 25V dc to tune a cap for use with an antenna.
Currently I can only get a steady 0v or 25V out of the device, the DAC has a 7 bit register and anything above 0 gives max output(25v)Checked the data being sent and everything looks correct, and have also read back correctly the register and the manufacturers ID.Any ideas? #smart-antenna-tuningWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.