2022-11-03 10:18 AM
Solved! Go to Solution.
2022-11-03 12:10 PM
Welcome, @PZuko.1, to the community!
Yes, you can do that.
For example, you can connect the STM8 to the PC via ST-LINK and use STVP to make the connection. STVP is included in the software package STVD, which should not be installed in C:\Program Files\ because of irritating spaces (STVD is still from the old Windows era), but as admin in a short path like e.g. C:\ST\STVD
In STVP there are three tabs at the bottom PROGRAM MEMORY, DATA MEMORY and OPTION BYTE, with which you can select the appropriate target area - so for the EEPROM area DATA MEMORY. If you have activated it, you can enter data directly in the EEPROM area, which can be written with
With Address Range you define the range to be written, e.g. 1000...100F, which is to be written instead of the entire tab range.
Does it answer your question?
Regards
/Peter
2022-11-03 12:04 PM
Yes, it is possible.
You can try with STVP.
2022-11-03 12:10 PM
Welcome, @PZuko.1, to the community!
Yes, you can do that.
For example, you can connect the STM8 to the PC via ST-LINK and use STVP to make the connection. STVP is included in the software package STVD, which should not be installed in C:\Program Files\ because of irritating spaces (STVD is still from the old Windows era), but as admin in a short path like e.g. C:\ST\STVD
In STVP there are three tabs at the bottom PROGRAM MEMORY, DATA MEMORY and OPTION BYTE, with which you can select the appropriate target area - so for the EEPROM area DATA MEMORY. If you have activated it, you can enter data directly in the EEPROM area, which can be written with
With Address Range you define the range to be written, e.g. 1000...100F, which is to be written instead of the entire tab range.
Does it answer your question?
Regards
/Peter
2022-11-03 1:02 PM
Hi,
Yes! this is exactly what i was looking for.
I need to dump flash and eeprom memory from one stm8 uP and write it to another one.
Many thanks!
2022-11-04 1:16 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2022-11-04 3:49 AM
The other more chilling issue with Program Files is that Microsoft really does not like apps writing into their directories there, and the multi-user, concurrently sense, which was common practice in earlier times. This and the Desktop have weird Virtual directories as Microsoft tries to manifest something like UNIX links.
Short paths, no spaces or weird characters is a much safer bet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.