2020-04-02 11:53 PM
Hi there!
I am new to STM8s Discovery, could someone suggests me how to print the values of variables in the program? it is more convenient if i can do this but I have no idea how to make it. Thank you very much !
Morris
Solved! Go to Solution.
2020-04-06 9:40 AM
Looking at your question again, maybe you didn't mean on-target debugging, but just plain old output from your program. If you want to do that: Set up an UART for serial output, provide a putchar protoype that uses it, then just use printf() like you would on any other C implementation.
For an example, see e.g. http://www.colecovision.eu/stm8/STM8S-DISCOVERY%20Serial.shtml (the example uses SDCC, but should work without changes for IAR, too, and only require minor changes for Cosmic and Raisonance).
2020-04-06 9:33 AM
The STM8S supports on-target debugging, so this should just work. AFAIK it is supported by all the usual development environments, be it STVD, or one from IAR, Cosmic or Raisonance.
If you use SDCC, you would do it by compile with --debug --out-fmt-elf to generate ELF/DWARF output that can then be used with OpenOCD and GDB for on-target debugging.
2020-04-06 9:40 AM
Looking at your question again, maybe you didn't mean on-target debugging, but just plain old output from your program. If you want to do that: Set up an UART for serial output, provide a putchar protoype that uses it, then just use printf() like you would on any other C implementation.
For an example, see e.g. http://www.colecovision.eu/stm8/STM8S-DISCOVERY%20Serial.shtml (the example uses SDCC, but should work without changes for IAR, too, and only require minor changes for Cosmic and Raisonance).
2020-04-08 9:16 AM
Hi Philipp,
Thanks for your reply!!!!
I have tried your suggestion and i am able to use printf() now!!!!!
Thanks a lot!!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.