2007-06-04 12:28 AM
2007-06-04 12:26 AM
I have a problem in my application which , I suppose , refers to wrong interrupts initialization.
In my program I have external interrupts , timer A interrupts , SCI ( UART interupts ) and in continuation - SPI interrupts. I don't exactly know how even to define my problem. The following scenario keeps repeating itself: - The program works , the interrupts are executed - I decide to tak step forward and made some change/ addition in the algorithm - The program stops wrokin correctly - I revert the changes i've made , but the program still doesn't work - After number of random corrections ( usually associated with interrupts ) the program starts working correctly again. - And from the beginning........ Is there any determine sequence for interrupts service initialization? Please help , the isuue is very urgent. I use ST72F321BAR9 micro I debug using InDART. :-? :-? :-?2007-06-04 12:28 AM
By now i have a problem adding SCI interrupt
Without SCI interrupt - external source interrupts work correctly :-[We’re moving the ST Community to a new platform to give you a better and more reliable community experience.