Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi all, I'm new to developing with the STM8 and noticed that the dlstm8smn.a library is taking up nearly 1kB of flash in my project. I'm wondering if someone could help demystify what all these object files are doing and where I could potentially opt...
I have posted already that I am using STM8152R8 nucleo board I have downloaded cosmic c compiler and it's license file too. I have also downloaded the STM8L library (en.stsw-stm8016) from the ST website. I have included the source files and include...
My stvd project settings panes for Compiler and to the right of it have font size too big. Consequentially I can only acess the top left of the pane. I need to change the const section address and I can't get to it, so my project is on hold until ...
Hello. I want to make the controller a slave for the SPI. I understand the hardware activation Support leg stm8 at present, as it was then activated receiving \ transmitting?/* Includes ----------------------------------------------------------------...
what's MSL OF STTH4R02S
Hello, I am trying to program a stm8l151c8 with Raisonance but I get the following message: Cannot communicate with the tool. Wrong tool selection or check tool power supply or check that a previous session is closed. Do I need to change any jumper o...
In order to create a gang programmer we were thinking of using multipe STM32 processors were every processor implements the SWIM interface in order to program STM8 processors in parallel. We can we find code written for a STM32 device which implement...
In an application we use PB4 as output. Corresponding to the datasheet, this port only can be used with open-drain. In the datasheet in the I/O port pin characteristics there are values of 30k up to 80k for pull-up resistor Rpu. Is this meant for the...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.