2003-11-05 5:34 PM
InDart ICP used some pins, is it unable to use ?
2003-11-03 3:02 PM
InDart used the following pins, ( ST7LITE09 )
If I want to use these pins, is it I cannot use InDart ICP ? Or I need to program the flash first PA5: ICC DATA PA6: ICC CLK PB4: ICC OSC_CLK2003-11-03 8:41 PM
You can use these pins in youe applcation if you only need to program the device, if you want to use the indart for in-circuit debugging then these pins have to be left at reset state and not modified by your application.
Hope this helps Regards sjo2003-11-03 10:15 PM
These pins are used when you are programming using ICC mode.
PB4: ICC OSC_CLK pin may or may not be used depending upon the option byte(ICP OPT disable/enable). After programming, you can use these pins as normal port pins unless you are not using these pins for in circuit debugging.2003-11-05 5:34 PM
Dear all, thank you very much.
^_____^ ~We’re moving the ST Community to a new platform to give you a better and more reliable community experience.