2003-04-03 2:11 AM
indart HDFlash : If (unsigned int>unsigned int) bug when in step mode
2003-04-02 4:18 AM
For your information, I found a bug in the indart-ST7 software V1.1.0 using the ST72521 indart kit (ST7F kit).
A corrected version should be available shortly on The If (unsigned int > unsigned int) instruction provides the opposite result than the one expected when using a HDFlash indart kit in step by step mode. In any other configuration ie - device only - HDFlash indart kit in run mode and no breakpoint - EMU3 from ST the code is correctly executed. The If (unsigned char > unsigned char) works fine in any of these configuration including HDFlash indart kit in step by step mode. Take care, Jojo2003-04-03 2:11 AM
Hi jojo,
thanks for finding the bug! New versions of the inDART software are available at ourhttp://www.softecmicro.com/download.html?type=browse&title=Software
. For inDART-ST7 users, download inDART-ST7 User Interface (v. 1.12) For inDART-STX for ST7 users, download inDART-STX for ST7 User Interface (v. 2.01) --PaoloWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.