2009-03-31 3:10 AM
In-Application Programming using UART my application doesn't work
2009-03-24 9:02 PM
Following the AN2078 I was able to connect my eval board for STR730 to PC serial port, I downloaded my application example pressing ''1'' inside HyperTerminal, but when I pressed ''2'' nothing happened.
I checked and read the programmmed Flash Memory: it seemed to be as described in application note at page 7 (User Application should start from 0x80002000 for STR73x series). Any idea?2009-03-31 3:10 AM
One step more!
Now I'm able to connect to RS232 and upload my Application; after that pressing ''2'' key my application starts. One big problem again: using application without interrupts and starting from 0x80002000 for vector table and 0x80002B90 for ROM all is OK. If I use one Application with Interrupts nothing work after uploading. Any idea? Is there a way to set correctly vector table and ROM start address when interrupt are used?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.