2009-10-14 10:07 PM
In-Aplication programming with uart not working
2011-05-17 12:50 AM
Can anybody give me some pointers on how to track down the cause of this problem. All I have been able to track down is that it keeps going to the reset line in the 91x_vect.s file. Is there any way of finding out why this is?
2011-05-17 12:50 AM
I am trying to get the In-Application Programming example working on our eval board using the IAR 4.42a workbench. It compiles and loads on to the board but does not get past the initialization program. When I ran the program with the debugger I found that it goes straight from program start to line 38 ( LDR PC, Reset_Addr) in 91x_vect.s. Has anyone else had this problem? If so how did you fix it?
[ This message was edited by: joshh on 29-02-2008 21:40 ]2011-05-17 12:50 AM
Did you follow the steps described in the STR9 In-Application Programming using UART application note(see attached file, section 1).
May you need also to use EWARM4.42A.2011-05-17 12:50 AM
I am using 4.42a. The 4.3 in the first post was a typo I did not notice. Is there anything special I need to do to have the program loaded onto bank 1 or is that already set up in the project files?
[ This message was edited by: joshh on 01-03-2008 20:28 ]2011-05-17 12:50 AM
You need first to remap the bank 1 to address 0 before loading the IAP.
You can use the JlinkSTR91x.exe utility to do this. See the following link: http://www.st.com/mcu/forums-cat-6333-21.html2011-05-17 12:50 AM
That fixed it. Thanks
2011-05-17 12:50 AM
Hello,
I am trying to run the IAP by usart. I could achieved to run the application for the ST's compiler systick example but i couldn't run it for any other code. I am converting the axf to bin and sending it via hyperterminal. It always fails in the 9th packet. Do you have any information about that? What must i do to use the IAP for any project. Thanks and Regards...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.