2006-01-30 3:56 PM
Idea of measuring RMS voltage and current using MCU ADC
2005-12-16 5:25 PM
Dear sir,
I have a project which needs to measure Supply Voltage and Current.I want to measure them using only MCu adc (ST7 with 10 bit ADC and 6 analog i/p channel).Could anybody help me ??I want a tested circuit and also want the idea/steps to develope this firmware to measure voltage and current rms value.I believe supply input voltage is always RMS if it is not mentioned.so i don't have to take voltage sample ,square ,take average and take root of it.Or do I??Pls correct me if i am wrong. pls note the max voltage and current for the system to measure are 260 V and 30 A respectively.And I know how to configure the adc for this particular MCU Thanks, arup2005-12-22 9:44 PM
Hi,
There will be soon an Application Note on this subject published on our web site. Best regards Laurent2005-12-22 11:03 PM
thanks for the info.what is expected time...could it be possible for you to tell about that.
regds, arup2006-01-30 3:56 PM
''Hi,
There will be soon an Application Note on this subject published on our web site. Best regards Laurent '' **************************************************** Dear Mr Laurent, Could you be able to give exact time frame ,atleast approximately, for this particular App Note to be available on this website. Thanks, ArupWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.